Skip to main content

Discover how geothermal heating systems capitalise on the Earth’s natural heat to deliver energy-efficient solutions for heating, cooling, and hot water, offering a renewable alternative to traditional HVAC systems.

As demand for renewable energy solutions grows, geothermal heat pumps (also known as ground source heat pumps) have emerged as a highly efficient option for home heating, cooling and hot water. By using the Earth’s stable underground temperature, geothermal systems deliver reliable comfort while reducing energy bills and carbon emissions. This guide explains how geothermal heat pumps work, their benefits and challenges, installation costs, and whether this renewable heating system is a worthwhile long-term investment for your home.

What are geothermal heat pumps and how do they work?

What is geothermal energy?

Geothermal energy is a renewable energy source that comes from the heat generated and stored beneath the Earth's surface. Leveraging the Earth's natural thermal energy, these systems offer an efficient, long-term solution for managing indoor climates, with a Seasonal Coefficient of Performance (SCOP) of 3 to 4 and the potential to cut CO₂ emissions by up to 90% compared to fossil fuel heating.[1]

Geothermal heat pumps, often referred to as ground source heat pumps, use the Earth’s stable underground temperature to provide heating, cooling, and hot water for homes and buildings. Unlike traditional HVAC systems, which rely on fluctuating air temperatures, geothermal heat pumps draw heat from the ground in winter and release it back during summer.

How do geothermal heat pumps work?

The operation of geothermal heat pumps is based on ground heat extraction through a series of underground pipes called ground loops. These loops, filled with water or antifreeze solution, absorb the Earth's consistent temperature - ranging between 5°C and 15°C year-round - and transfer it to a heat pump inside the building. In winter, the system absorbs heat from the ground and moves it into the building. In summer, the process reverses, drawing heat from the building and dissipating it into the ground.

Because underground temperatures remain relatively stable throughout the year, geothermal heat pumps maintain consistent performance even during cold winters and heatwaves.

While air-source heat pumps are also highly efficient and designed to operate across a wide range of outdoor conditions, geothermal systems benefit from being less exposed to seasonal temperature fluctuations. Compared with fossil-fuel heating systems, both technologies offer a more energy-efficient and lower-emission approach to home comfort.

The benefits of geothermal heating systems

1. Energy efficiency and cost savings

Geothermal heating systems are renowned for their high energy efficiency. Rather than generating heat through combustion, geothermal heat pumps transfer existing heat from the ground, reducing energy consumption while maintaining comfortable indoor temperatures throughout the year.

Key efficiency benefits include:

  • High seasonal performance: Geothermal heat pumps typically achieve a Seasonal Coefficient of Performance (SCOP) of 3 to 4. This means that for every unit of electricity consumed, the system delivers 3 to 4 units of heating or cooling energy.
  • High Seasonal Performance Factor (SPF): Geothermal heat pumps maintain a higher SPF over the entire heating season, ensuring consistent performance even in extreme weather.
  • Lower energy bills: Homeowners can reduce heating and cooling costs by 20% to 60% with geothermal HVAC systems. Over a 15- to 20-year lifespan, the savings on energy bills far outweigh the higher initial installation costs.

Although installation costs are generally higher than those of conventional heating systems, lower running costs can help offset the initial investment over time. In addition, installing a renewable heating system such as a geothermal heat pump may improve a property's attractiveness to future buyers, particularly as energy efficiency and sustainability become increasingly important considerations.

2. Environmental benefits

Geothermal systems are a cornerstone of green heating technology, contributing to greenhouse gas reduction and the transition to renewable power sources:

  • Reduced emissions: Geothermal heat pumps produce no direct emissions, significantly lowering carbon footprints compared to fossil fuel systems. During the use phase, they can reduce on-site CO₂ emissions by up to 90% compared to natural gas or oil heating systems, based on typical SCOP performance and an average European grid electricity mix.[1]
  • Minimised fossil fuel dependence: By tapping into renewable ground heat, geothermal systems reduce reliance on non-renewable energy sources, supporting energy security and a lower-carbon energy supply.


3. Durability and low maintenance

  • The components of a geothermal HVAC system are designed for longevity:
  • Ground loops can last 50+ years.

4. Quiet and discreet installation

Unlike air-source heat pumps, geothermal systems do not require a visible outdoor unit, helping preserve outdoor space and reduce visual impact.

Because most of the system is located underground and indoors, geothermal heat pumps operate quietly compared with many conventional heating systems. The absence of an outdoor fan unit can be particularly beneficial in noise-sensitive locations or properties where aesthetics are a priority.

Types of geothermal systems

Geothermal systems are adaptable to various property types and geographical conditions. The most common configurations include:

  • Closed-loop systems:
    • Horizontal loop ground source heat pumps are installed in shallow trenches and are suitable for properties with ample space.
    • Vertical loop ground source heat pumps use boreholes drilled deep into the ground and are often preferred for smaller plots.
  • Open-loop systems: These systems use groundwater directly as a heat source or sink, making them highly efficient but dependent on water availability.
  • Hybrid systems: Combine geothermal technology with other renewable power sources, such as solar, to optimise energy efficiency.

Installation process and costs

Installing a geothermal heating system involves several key steps:

  1. Site assessment: A detailed evaluation of the property’s heating and cooling requirements, soil conditions, and available space.
  2. System design: Determining the appropriate system type (closed-loop or open-loop) and configuration (horizontal or vertical).
  3. Drilling and loop installation: Ground loops are installed underground. Vertical systems require deep drilling, while horizontal systems involve trenching.
  4. Heat pump installation: The indoor heat pump is connected to the ground loop system and building ductwork.
  5. Testing and commissioning: Ensuring the system operates efficiently and meets the building’s heating and cooling needs.

Geothermal heat pumps can be installed in both new-build homes and renovation projects, although installation requirements vary depending on available land, soil conditions and the existing heating system.

The upfront cost for a residential geothermal system ranges from €15,000 to €30,000. While higher than traditional HVAC systems, government incentives and long-term savings on energy bills can offset these costs.

Challenges of geothermal heat pumps

While geothermal systems offer numerous benefits, they come with challenges:

  • High initial costs: The upfront investment can deter homeowners, even though the system pays for itself over time.
  • Space requirements: Horizontal loop systems require significant land area, which may not be available for all properties.
  • Site limitations: Factors like rocky soil or limited groundwater access can complicate installation.

Ground source heat pumps vs. air-to-water heat pumps

FeatureGeothermal heat pumpsAir-to-water heat pumps
EfficiencyHigh (SCOP: 3 - 4)High (COP: 2 - 3)
Operating costsLowModerate
Dependence on outdoor climateMinimalHigh
Lifespan15–20 years

10–15 years

Initial installation costsHighModerate

Unlike air-source systems, which rely on outdoor temperatures, geothermal systems benefit from the Earth’s constant underground temperature, ensuring constant performance year-round.

Want to know more? Find out how to choose between an air-to-water heat pump and a ground-source heat pump or discover our air-to-water heat pumps.

How can geothermal systems cut energy bills?

Geothermal systems drastically reduce energy bills by using renewable ground heat extraction instead of generating heat through combustion. According to studies:

  • Heating and cooling costs can drop by 20% to 60% compared to systems that generate heat through combustion.
  • Households switching from traditional systems to geothermal can save hundreds of euros annually.

The combination of high efficiency, low operating costs, and durability makes geothermal HVAC systems a cost-effective choice for homeowners.

What is the environmental impact of geothermal energy?

During the use phase, geothermal systems produce significantly lower on-site greenhouse gas emissions than fossil-fuel-based systems, helping to reduce homeowners' carbon footprint. By relying on the Earth’s natural heat, they also reduce dependence on finite energy resources.

Furthermore, the underground components of geothermal systems minimise their impact on the landscape and ecosystem.

Is a geothermal or ground source heat pump worth it?

Before deciding to invest in a geothermal heat pump, it’s critical that you evaluate property suitability, including space and soil conditions. Explore government incentives such as grants to help with installation costs and weigh up long term savings and environmental benefits over upfront costs.

Ultimately, the decision to invest in a geothermal system depends on individual circumstances:

  • For homeowners seeking to reduce their home's carbon footprint: Geothermal HVAC systems can cut carbon emissions by up to 90% compared to traditional gas boilers, making them an excellent choice for those committed to lowering their environmental impact.
  • For long-term planners: The upfront cost pays off over time through lower energy bills and minimal maintenance.
  • For properties with adequate space: Homes with sufficient land for ground loops are ideal candidates for geothermal systems.

The future of geothermal heating systems

Geothermal heating systems represent a significant step toward reducing reliance on fossil fuels for home heating. By offering a SCOP of 3 to 4, energy bill savings of 20% to 60%, and CO₂ emission reductions of up to 90% compared to fossil fuel systems, they have become a leading renewable heating technology. As the world continues its transition to renewable energy, geothermal systems will play an important role in reducing the carbon footprint of home heating. With their potential to cut energy bills and reduce greenhouse gas emissions, geothermal heat pumps are not just an investment in your home - they're an investment in a lower-carbon future

FAQs about geothermal heat pumps:

1. How does a geothermal heat pump work?
A geothermal heat pump is an energy-efficient system that uses the stable temperature of the earth to heat and cool buildings. It transfers heat to or from the ground via a series of buried pipes (ground loops) and a heat exchange system. During winter, it extracts heat from the ground to warm your home, and in summer, it removes heat from the home and transfers it into the ground.

2. Where can geothermal heat pumps be used?
Geothermal heat pumps can be used almost anywhere, as the ground maintains a consistent temperature year-round, regardless of the surface climate. They are suitable for residential, commercial, and industrial applications, and can be installed in urban, suburban, or rural locations.

3. How energy-efficient are geothermal heat pumps?
Geothermal heat pumps are extremely energy-efficient. Geothermal heat pumps typically achieve a SCOP of 3 to 4, meaning that for every unit of electricity consumed, the system delivers 3 to 4 units of heating or cooling energy. This is because they move heat rather than generating it, making them more efficient than traditional heating and cooling systems.

4. What are the installation costs for a geothermal heat pump?
The initial installation cost for a geothermal heat pump range from €15,000 to €30,000. However, government incentives, as well as long-term energy savings can make it a cost-effective investment over time.

5. What maintenance does a geothermal heat pump require?
A geothermal heat pump requires regular maintenance to ensure it runs efficiently and lasts a long time. This includes having a qualified engineer to service the heat pump annually to check the refrigerant levels, inspect system components, and inspect the ground loops.

6.Is a geothermal heat pump the same as a ground source heat pump?
Yes. The terms geothermal heat pump and ground source heat pump are often used interchangeably. Both systems use the stable temperature below the Earth's surface to provide efficient heating, cooling and hot water.

Conclusion: Are geothermal heat pumps worth it?

Geothermal heat pumps, also known as ground source heat pumps, provide highly efficient, low-carbon heating, cooling, and hot water by leveraging the Earth’s stable underground temperature. They deliver significant energy savings, reduce carbon emissions by up to 90%, and offer long-term durability, with ground loops lasting over 50 years.

While installation costs are high and space requirements can be challenging, government incentives and lower operating costs make them a cost-effective investment over time. As the world transitions to renewable energy, geothermal technology stands out as a key solution for greener, more resilient homes and a sustainable future.

Key takeaways

  • Geothermal heat pumps use the Earth’s underground temperature to provide heating, cooling and hot water for homes and buildings.
  • Key benefits: energy efficiency, cost savings, environmental benefits, durability and low maintenance.
  • Key challenges: high initial costs, space requirements and site limitations.
  • Three main system types: closed-loop systems, open-loop systems and hybrid systems.
  • As the world continues its transition to renewable energy, geothermal systems are expected to play an important role in a more sustainable future.

Ready to see if geothermal heating is right for your home?

[1] Ground source heat pump carbon emissions and primary energy reduction potential for heating in buildings in Europe – results of a case study in Portugal, Renewable and Sustainable Energy Reviews, 2015.