Skip to main content

The indoor temperature we live and work in can dramatically affect your sleep, focus, mood and long-term health

Couple playing board games while enjoying a perfect room temperature

When a room feels cold or has stuffy air quality, we’ll tend to start feeling sluggish or our mood will drop. But do you know about the many ways in which the ideal indoor temperature of your home can affect your physical and mental health?

 

What is a recommended comfortable room temperature? The ideal indoor temperature isn't just about comfort – it can have a real effect on your physical and mental health. Be it body temperature, cognition, resistance to infection, mental health or even dementia symptoms, your home's temperature makes a big difference to your well-being.

Degrees of well-being

Ambient indoor temperature may seem like a minor factor in your general peace of mind, but think back to the last time you were in a place that was too hot or cold. It might be an event in an uncomfortably warm venue or a working day in an overly chilled office. Think about how much it affected not only your happiness but your performance.

According to GBCSA and a study done by Nurick and Thatcher, thermal comfort influences mood, efficiency, productivity and work satisfaction. Too hot? Employees feel sluggish and tired. Too chilly? They struggle to concentrate. Studies at Helsinki University of Technology and the Lawrence Berkeley National Laboratory back this up: scientists found that employee productivity was highest at 21-22°C. Each rise of 1°C causes a fall in productivity by 2 percentage points.

What is a healthy indoor temperature?

If your house is cold and damp, it becomes a breeding ground for damp and mould. An indoor temperature of less than 16°C increases the risk of asthma and other respiratory conditions, while going below 12°C puts the cardiovascular system under stress. A cold home can increase your risk of depression and confusion. If you are living with chronic pain, it can make conditions much worse. If it's too warm and stuffy, we can develop headaches or irritated mucus membranes, or we might feel too tired to concentrate.

What is a recommended comfortable room temperature?

So, what’s the recommended indoor temperature? It depends on the room, but 20°C is a good baseline. Bathrooms should be warmer, between 22 and 24°C, to avoid a shock when you step out of a hot shower. Adults’ bedrooms need to be cooler, between 16 and 19°C, as our body temperature decreases as we sleep. We sleep better if our internal regulatory system doesn't have to work too hard. Bear in mind, though, that an overly cold bedroom can be hard to sleep or study in if it doubles as a student’s work area.

Children’s bedrooms should be around 17-20°C. If a child’s room is too hot, and therefore has dry air quality, it can lead to respiratory problems. For older people sleeping in a too-warm bedroom has been said to contribute to heart attacks, asthma and stroke. Studies have shown that physical performance in elderly people – from their ability to get up from a chair to how quickly they can walk – is negatively affected by a hot ambient temperature.

Balanced temperature, better life

Living, working and sleeping at the ideal temperature gives your body one less thing to worry about. If you’re not having to regulate your temperature continually, you can use that energy for other things.

Choose the right indoor thermometer

Having a reliable indoor thermometer is essential for maintaining control over your indoor temperature. A digital thermostat is highly recommended because it provides accurate and sensitive readings, allowing you to monitor the indoor temperature precisely.

Daikin's solutions are designed to assist you in achieving the ideal indoor temperature, promoting comfort and well-being for you and your family throughout the day and night. Our systems ensure that your living environment remains consistently comfortable, supporting a healthier and more enjoyable indoor atmosphere.

Room-by-room: what’s the ideal temperature?

Different rooms serve different purposes, and require different settings.

Room

Ideal temperature

Living spaces

20–21°C

Bathrooms

22–24°C (warm enough to avoid post-shower chills)

Adult bedrooms

16–19°C (cooler for optimal sleep)

Children’s rooms

17–20°C

Elderly residents

~20°C stable temperature (to reduce health risks)

A smart home is a healthy home

Maintaining the right indoor temperature consistently — throughout changing seasons — is key. Most people perform and feel best around 20–22°C, while both colder (<16°C) and hotter (>26°C) environments increase health risks.
Heat pumps, especially when paired with smart thermostats, allow you to maintain this balance year-round. They provide stable heating and cooling while helping improve energy efficiency and overall indoor comfort.
Creating a healthier indoor climate starts with control, consistency, and the right system design.

Key takeaways

  • An indoor temperature of 20-22°C is healthiest and most comfortable for most people.
  • Both cold (<16°C) and hot (>26°C) indoor environments increase health risks, especially for vulnerable groups.
  • Productivity can drop by up to 2% for every degree above 22°C.
  • Different rooms require different ideal temperatures, such as 16-19°C for bedrooms and 22-24°C for bathrooms.
  • Smart thermostats and heat pumps help efficiently maintain a stable, healthy indoor climate.

Discover how Daikin solutions help you create a healthier indoor climate — talk to a specialist about system design, zoning, and HVAC solutions.