Skip to main content

How to make the most of available grants when installing a heat pump

At first glance, heat pumps may appear to require a larger initial investment compared to traditional heating systems. However, when considering the purchase of a heat pump, it is important to know that the chances of premiums are high which make investing in a heat pump very attractive.

In an effort to combat climate change, many governments have decided to phase out gas and oil boilers. Instead, they are encouraging the adoption of low-carbon solutions such as heat pumps.

Historically, convincing homeowners to make the switch to heat pumps has posed a significant challenge. However, rising gas prices are becoming a concern across Europe and subsidies are now available in most countries. Because of this, there is growing enthusiasm and recognition that heat pumps are a viable option.

Subsidies play a crucial role in enhancing the competitiveness of air-to-water and ground-source units. By incentivising the adoption of these technologies, the transition towards sustainable heating solutions can be further accelerated.

For detailed data, sources, and references, please refer to the full whitepaper (available for download in English).

More reasons to choose a heat pump