Skip to main content

Independent air conditioner installers experienced with Daikin systems are ready to deliver

So you've decided a heat pump is the future-proof way of heating your home. Now you're looking for a heat pump installer near you, to discuss your project and get a price quote. Daikin is here to help.

STEP 1: FILL IN THE FORM

Thank you for filling in the form below. It helps us to connect you to an independent installer for your new heat pump.

Please include important details about your project:

  • Tell us how many rooms you are planning to cool or heat.
  • Explain what you're planning. Is it a new installation? Planning a renovation? Or building a new home?
  • Maybe you've spotted a Daikin product that looks right for you. Feel free to let us know which product interests you.

With this information, we can match you to the perfect heat pump installer for your project.

STEP 2: WE MATCH YOU TO AN INSTALLER NEAR YOU

Great! By filling in the form, you've taken the first step to heating and cooling your house with an air conditioner. Here's what happens next.

First, we match you to an independent installer experienced with Daikin products near you.

We select an installer based on these criteria:

  • They are an experienced installer of the product you have in mind
  • They are available for new projects
  • They are close to you
  • They have the best feedback score

Please allow a few days for us to match you to the heat pump installer.

One or two working days after you fill in the form, we'll email you the name of the best installer for your project.

STEP 3: THE INSTALLER CONTACTS YOU

A few days after you receive your installer's name, they will contact you to arrange a site visit. (Of course, if you prefer, you can contact the installer yourself, once you receive their details.)

STEP 4: THE SITE VISIT

A site visit allows the air conditioner installer to understand your needs and the possibilities of your home. With that information, we can propose the best product for your needs.

The installer will check:

The energy efficiency of your house, as well as any limitations or regualtions regarding your building or home.

Your existing system and needs. How large is your house? Which rooms need cooling, heating, ventilation or air purifiers? How many heating elements do you have in your house? How powerful are they?

Your lifestyle. How many people live under your roof? How often are you at home? What is your preferred temperature inside the room?

Practical information for the AC installation. The certified installer will check where to install outdoor and indoor units and where to lay the piping.

If you have questions, the site visit is the best time to ask them. Some of the questions you might want to ask are:

  • Is a heat pump right for me? Your installer can help you, by discussing your needs and expectations, your existing setup and also the financial implications, to decide if a heat pump is the right solution for you.
  • Which type of heat pump is most suitable for my home? The installer can explain the different types of heat pump and their costs and installation procedures, to help find out which is best for you. 
  • Do I need any additional building works for a heat pump to work efficiently? At the visit, your installer may suggest some steps you can take to maximise your heat pump's efficiency, especially if you live in an older building.
  • What capacity heat pump do I need? To recommend the right capacity heat pump for your needs, your installer will consider the size of the property, along with several other factors including its age and its energy efficiency. This will ensure your heat pump provides precisely what your home needs, no more and no less.

STEP 5: THE PRICE QUOTE

Shortly after the site visit, the heat pump installer will send you a quote for your desired solution.

In the offer you will find:

  • The price of the Daikin products: the price of the outdoor unit, the indoor unit and the controller.
  • Optional extras that may be suggested for your area, for example anti-corrosion treatment for coastal areas.
  • The price for other materials needed for the job: the piping and any other parts necessary to install your heat pump
  • The price of installation: the work that goes into installing your heat pump

Additionally, the installer might offer you a maintenance contract or extended warranty.

STEP 6: THE AIR CONIDTIONER INSTALLATION

Once you accept the quote, you can count down to the day your new air conditioner is installed.

Tip: Order well in advance. Particularly as summer nears, installers can be very busy. The installation of your heat pump itself is quick: it usually takes just one or two days to install your AC and switch it on.

These are the steps your certified installer will typically take to install the outdoor unit of your heat pump system:

  • Choose the best place: the installer will take into account how strong the surface is and how much space there is around the unit
  • Place the unit: it must be securely fastened on a completely level surface, ideally on blocks, with space at the top for maintenance
  • Install the drain: a drain plug allows the installer to drain the outdoor unit
  • Widen the end of the pipes: the end of the piping is cut, deburred and widened
  • Fix the refrigerant pipes: union nuts are used to attach the widened sections of the pipes
  • Check for gas leaks: once the pipes are connected, the installer vents the unit and checks for gas leaks
  • Fill with coolant: in Daikin heat pumps this is usually the refrigerant R-32, which is filled in liquid state through the gas pipe
  • Connect the cooling pipes: the installer uses a special pipe bender and is careful to make sure no moisture or dust gets into the pipe
  • Electrical wiring: the electricity is connected and an earth leakage detector and circuit breaker are fitted
  • Trial run and testing: the installer measures the supply voltage and tests the system in both cooling and heating mode

STEP 7: YOUR AIR CONDITIONER IS READY TO GO

Now you can enjoy optimal indoor temperatures all year round, plus support from Daikin whenever you need it.

Congratulations, you are now a heat pump owner! You no longer need fossil fuels to heat your home. You are now part of the future of heating.

Onecta app: Get complete control over your heating and cooling systems – wherever you are, and in whatever way works for you – with our Onecta app.

With Onecta, you can set temperature schedules, change the operation mode, and review your energy consumption with an easy-to-use app on your phone – or via your voice-activated Alexa or Google Home assistants. You can even control multiple rooms in several homes or monitor the outdoor air quality and pollen levels. All you need to do is install the app, sharing access with your family and friends if you wish, and you’re good to go.

Download Onecta here.

Warranty packages: The quality of our products is second to none, but in the unlikely event that a problem does occur, you don’t need to worry. All our domestic products come with a three-year guarantee as standard. All Daikin South Africa warranties are supported by our installers.

Our additional warranty packages cover your devices for up to 10 years, so you don't need to worry about anything going wrong over the longer term. If it does, we'll take care of it for you.

So you can relax and enjoy complete peace of mind that any technical issues will be covered. How's that for service?

Daikin works with independent installers experienced with Daikin systems close to you. However, we're always available to answer your questions. Don't hesitate to contact us if you would like more information or help.